Affected Versions
- exacqVision Web Service 7.6, running on Windows
<br>
Description
In web service 7.6 (Windows only), dewarping of Dahua fisheye cameras does not work. These cameras do not show any dewarping options in the web client or Exacq Mobile 3 app.
<br>
Workaround
- Install the exacqVision Client on the web service or refer to an existing client installation on another machine.
- Copy C:\Program Files (x86)\exacqVision\Client\fish_eye.dll where the client is installed to the C:\Program Files (x86)\exacqVision\WebService\bin directory where the web service is installed.
- Restart the web service.
<br>
Resolution
Update exacqVision Web Service to version 8.2.2 or higher
<br>