Panasonic overrides smartcoding setting

Description

Panasonic plugin always default to “framerate” priority setting when connects to the camera. This overrides any other settings (VBR/VBR+SmartCoding/Best? Effort/Advanced? VBR) that the user might want to set through the camera web interface. This became an issue when Coca Cola has a need to set their cameras to VBR with SmartCoding? and was being override to “framerate” instead.


The fix is to allow the user to change the priority setting but maintain the recommended biterate with quality settings from the client. The expected change is listed in the table below.