Skip to content

Exacq

Support Portal CMS

Linux Doesn’t Remove Dynamically Assigned IP Addresses When NIC Unplugged

Description

Linux doesn’t drop network configuration when a dynamically-assigned NIC is unplugged as Windows does. However, if the package ifplugd is installed then it will.

Published May 4, 2021By Bhargav Atturu
Categorized as Knowledge Support, Support, Categories, Products, exacqVision Integrations Tagged Level2, NIC Unplugged, Linux doesn’t remove dynamically assigned IP addresses, IP Addresses, 5199

Post navigation

Previous post

Application does not show video panel after sidebar navigation from live focus page

Next post

iOS Application crashes when decoding H.264 video from Axis M5014 in 800×450 resolution

Recent Posts

  • Windows 7 Remote Connections
  • Associations Not Allowed to be saved as Momentary or Sustained Option
  • AVCostar (Arecont) AV20576RS camera model fails to decode H265 in ExacqVision
  • Illustra Edge Analytics
  • Hanwha Edge Analytics
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
  • Remote Connection