Getting server lists for exacqVision Client may connect to a server more than once

Description

If there are two different servers with the same server name in two different groups in ESM, it is possible that the client sync with ESM will pull in the server at different times during the continuous sync with ESM (every 5 minutes) by confusing the group hierarchy of the same named servers.

To workaround this, just insure servers are named differently.