Web service cannot connect to multiple servers at the same address

Description

If web service with more than one server at the same address, but different ports, those servers are not treated independently. When accessing these servers through the web service, only the first will handle requests.

<br>

Version Introduced

7.5.32

<br>

Platform

All

<br>

Steps to reproduce

  1. Configure two servers at the same IP with different ports (e.g. using a router).
  2. Add those servers to the web service.

Expected result

Both servers are handled as separate entities.

<br>

Actual result

The servers are handled incorrectly in the web service, not always using the correct server.

<br>

Work Around

Set up separate DNS entries for each server (i.e. give a unique address for each).

<br>

Version Fixed

none