Description
The ePlayer shortcut is missing from the menu. The player is still there and can be launched from the command line
<br>
Version Introduced
7.9.20
<br>
Platform
Linux
<br>
Steps to reproduce
- Install client deb
<br>
Expected result
- ePlayer shortcut under Exacq menu
<br>
Actual result
- Only client shortcut under Exacq manu
<br>
Work Around
- Run ePlayer from commandline
- Downgrade to 7.8
- Run sudo xdg-desktop-menu install /usr/local/exacq/client/share/exacq-progs.directory /usr/local/exacq/client/share/exacq-player.desktop
<br>
Version Fixed
8.0.3 (when it comes out)
<br>
Keywords
eplayer, e-player, shortcut