Streams not closed when recording is disabled

Description

With Dahua/Illustra Essentials, video continuous to stream when the recording for the stream is disabled in the ip camera recording page. Most likely this does not affect user but it affects traffic on the network.

<br>

Version Introduced

r71495 (6.8.x RC)

<br>

Platform

All

<br>

Steps to reproduce

disable stream recording in the “Recording” tab of the ip camera setup page.

<br>

Expected result

video stopped stream.

<br>

Actual result

video continuous to stream.

<br>

Work Around

disable/enable the device.

<br>

Version Fixed

None

<br>

Keywords

DahuaIpPi, Dahua