IPCamDetect crashes on Una server when camera disconnected from port during discovery/addressing

Affected platforms

exacqVision Server 7.4 on Una LC servers

<br>

Description

When a discovery scan and auto-addressing is interrupted by unplugging a camera from the Una POE ports or the port is power cycled, IPCamDetect could crash. This can happen when a camera is connected to one of the UNA ports, which triggers an auto scan on the port. Then during the auto-addressing, the camera is unplugged.

<br>

Workaround

None

<br>

Resolution

Update exacqVision Server to version 7.6.2.94278 or higher