Skip to content

Exacq

Support Portal CMS

ONVIF plugin memory leak: Motion and alarm events received via metadata streaming could cause crash

Affected platforms

exacqVision 5.4 or later

<br>

Symptom

When certain cameras are connected using the ONVIF plugin and the plugin is configured to use metadata streaming to receive motion and alarm events, a memory leak is possible. If memory usage increases enough exacqVision can crash. The crash is typically in ntdll which show a heap memory issue.

To validate this issue is the root cause of a crash, stop the Onvif plugin from requesting a metadata stream as described in the workaround.

<br>

Workaround

Edit the /exacqVision/server/onvifnvcpi.json file to remove the manufacturer’s entry. This will result in the loss of motion-based recording, so modify the recording schedule to use free run recording.

<br>

Resolution

No fix at this time.

Published April 28, 2021By Bhargav Atturu
Categorized as Knowledge Support, Support, exacqVision Server, Categories, Products Tagged Level2, 4951, Plugin Memory Leak, Motion Events, Alarm Events, Metadata Streaming, Server Software, Server, Plugin, Crash, Onvif

Post navigation

Previous post

Video Not Recording to iSCSIĀ  with Status “Recording Not Possible”

Next post

Unable to bookmark some events

Recent Posts

  • Synchronize with Enterprise Manager authentication – Connectivity error:500
  • Exacq Mobile Application Views show Black Box
  • Using an Axis D3110 Connectivity Hub with the Axis C1410 MK11 Speaker
  • FLIR Camera Motion Stops Recording Motion Events
  • exacqVision 25H1 Release Bulletin