The status of an input on USB module not updated if already connected when module plugged into server

Affected platforms

exacqVision 5.6.0 to 7.0

<br>

Symptom

When a new usbdio board is detected while the server is running, and it already has an input plugged in, the status of the input will not be updated in the client.

<br>

Workaround

Restart the exacqVision server. This will result in a brief interruption of video recording during the restart.

<br>

Resolution

Update exacqVision to 7.2 or later.