Rotary Menu Dismisses when no Actions are Available

Description

When no actions are available for a zone the rotary menu is dismissed.

<br>

Tested Version

  • Exacq Mobile 3, version 9.0.1

<br>

Platform

[All]

<br>

Steps to reproduce

  1. Add an association for a partition that is armed and has child zones.
  2. View the association on the live page.
  3. Tap to navigate to the live focus page.
  4. Tap to open the rotary menu.

<br>

Expected result

The rotary menu opens.

<br>

Actual result

The rotary menu closes.

<br>

Work Around

Remove the associated zone from the camera.

<br>