Internal memory leak when sending email

Affected platforms

exacqVision 4.12.3 to 7.0

<br>

Symptom

There is a small memory leak whenever the server executes a program. This leak is unlikely to cause a problem on any desktop systems, but it could cause a hang or reboot on Edge systems with limited memory, if the Edge server is configured to send frequent emails.

<br>

Workaround

Disable email notifications

<br>

Resolution

Fixed in exacqVision 7.2