Illustra discovery for Pro and Essentials issues with dual nic as well as Una systems

Inconsistent results. Web interface not showing all details, firmware, model, etc. Doesn’t always find Pro cameras even though static IP addressed. Also found 610LT’s twice and added them twice.

Workaround suggested

For Dual nic systems:
For dual nic systems with duplicated results, either disable one of the nic’s or make sure that they are not set to the same subnet.

For Una:
With UNA the camera HAS to be factory defaulted to be discover-able (this is a requirement for UNA to work). Either that or the camera has to be set to dhcp with dhcp support on the una ports. If the camera is set to static and is on a different subnet we may not be able to discover it.