ESM returns error when entering a rule duration using a decimal

Affected platforms

ESM 3.2 or later

<br>

Symptom

If the user enters a value using a decimal (for example, 10.5) for the duration value of a rule, ESM returns an error page when the user attempts to create the rule.

<br>

Workaround

Enter a valid integer (not a decimal number) between 1 second and the number of seconds in a year, which is about 31536000 seconds.

<br>

Resolution

No resolution at this time.