ESM does not uniquely display multiple groups with the same name in rules engine

ESM does not uniquely display multiple groups with the same name in rules engine

Effected platforms

ESM 2.6 or greater

<br>

Symptom

When multiple groups with the same name exist, the user may not be able to discern the individual groups when creating rules.

On ESM versions before 3.6, all the servers that are on groups with the same name would be listed under a single displayed group on the server dropdown.

On ESM 3.6 or greater, if the number of servers on ESM are less than 500, the behavior is the same as above. If there are more than 500 servers on that ESM, the user has to click on the group in order to see the servers belonging to it, and clicking on this group shows only servers in one of the groups with that name. It doesn’t show servers in the other group that shares the same name.

<br>

Workaround

Rename groups to have unique names.

<br>

Resolution

None at this time.