Server Email Notifications Broken

Symptom:

Server fails to send email notifications.

Problem:

This issue was introduced with trunk 9.7.15, server will fail to send notification. 

Server logs may show the following:

10/8/2018 9:41:30 AM     NotifyPI     Error     Failed to execute curl smtp operation using server gmail. (Profile Description: Gmail Profile)

10/8/2018 9:41:30 AM     NotifyPI     Error     Failed to send notification using profile Gmail Profile.  
This message will NOT be retried due to failure return codes 67 or 26 or due to failures to prepare or initiate email operation

Solution:

Update to server version 9.7.32 or higher.