PoE Interfaces Created on Non-PoE Server

Symptom:

After importing a configuration file, PoE interfaces appear on a machine with no PoE interfaces.

<br>

Problem:

Configuration exports are primarily intended for backing up configuration of the same machine, not for migrating a configuration to another piece of hardware.

When importing a configuration file from a PoE capable device (M-series or Una LC), to a machine without these interfaces the configuration file imports the interface settings for the PoE ports as well.

<br>

Solution:

Fixed in exacqVision Server version 9.4.