Duplicate cameras returned in the camera scan results

Affected platforms

exacqVision Server 7.2.0

<br>

Symptom

If multiple NICs are installed on the exacqVision server and one or more NICs are disconnected from the network, the camera scan may list the same camera more than once in the results.

<br>

Workaround

Connect the NIC in the disconnected state or disable the disconnected NIC.

<br>

Resolution

Update to exacqVision Server 7.2.2.86862 or higher