Article for IE Display Problems with Filtering

Description

When using IE 11 to run ESM, there’s a number of concerns regarding filtering functionality
– Clear filter button is never displayed
– Radio buttons on the filter dialog do not toggle off (issue with one of the javascript functions)

<br>

Tested Version

4.9.22

<br>

Platform

All

<br>

Steps to reproduce

  1. Navigate to any list view
  2. Open filter dialog
  3. Click on radio buttons next to a field
  4. Enter filter criteria
  5. Click Apply

<br>

Expected result

-Radio buttons can be turned on one at a time
– Clear filter button is displayed after dialog is closed

<br>

Actual result

– Radio buttons next to date filters do not function
– Clear filter button is displayed when filter criteria are entered

<br>

Work Around

Use Chrome or Firefox