Skip to content

Exacq

Support Portal CMS

System watchdog after changing time on an Una

Una systems may watchdog after changing the system clock backwards.

To disable usbdio watchdogs, add this to usbdio.ini:

watchdog=0

If Una is the 16 port version, the above line will need to be added to both device sections in usbdio.ini.

Published April 23, 2021By Bhargav Atturu
Categorized as Knowledge Support, Support, exacqVision Server, Categories, Products Tagged Changing Time, Level2, 4634, Una LC-Series, System Watchdog, Changing Time on Una

Post navigation

Previous post

Illustra3 cannot update ptz preset name

Next post

ESM downgrade fails with newly added users

Recent Posts

  • Synchronize with Enterprise Manager authentication – Connectivity error:500
  • Exacq Mobile Application Views show Black Box
  • Using an Axis D3110 Connectivity Hub with the Axis C1410 MK11 Speaker
  • FLIR Camera Motion Stops Recording Motion Events
  • exacqVision 25H1 Release Bulletin