Some Disks May Be Reported Twice In Server Storage Management Functions

Some hard disks may be reported twice in Windows, which may manifest in one or more of the following conditions:

  • One instance can indicate a storage alarm, while the other does not.
  • The non-alarmed instance may be the only one shown in the client, leading the user to believe that there are no storage alarms.
  • Both instances will be seen by ESM, and therefore ESM indicates a storage alarm.
  • Alarm states will be inconsistent between client, ESM and event linking. 

This affects exacqVision Server versions 8.2.0 through 9.9.16


To resolve this issue, update exacqVision Server to version 9.9.17 or higher.