Panels repopulate after clearing on server initialization failure

Description

After opening the application if the panels are cleared before a server initialization fails the panels are repopulated.

<br>

Version introduced

  • Exacq Mobile 3, version 8.1.12

<br>

Platforms

Mobile – All

<br>

Steps to reproduce

On Exacq Mobile 3

  1. Open the application
  2. Navigate to the Configure Web Service page
  3. Add a server that will fail to connect
  4. Return to the views page
  5. Select a camera for one or more panels
  6. Close the application
  7. Reopen the application
  8. Clear panel(s)
  9. Wait For server initialization to fail

<br>

On Browser

  1. Open the application
  2. Navigate to the Configure Web Service page
  3. Add a server that will fail to connect
  4. Return to the views page
  5. Select a camera for one or more panels
  6. Refresh the page
  7. Clear panel(s)
  8. Wait For server initialization to fail

<br>

Expected result

The panel(s) remain cleared

<br>

Actual result

The panel(s) are repopulated

<br>

Workaround

Clear the panels after the server initialization has failed.

<br>

Version fixed

Unknown.

<br>