ESM downgrade fails with newly added users

Description

Downgrading ESM from 4.5.10 or newer down to 4.5.9 or earlier can cause the following error. Also the installer fails not able to communicate with database.

ERROR [installer:74] Exception in run_backward_migrations: Traceback (most recent call last):

File "", line 40, in run_migration_command
File "south_utils\run_migrations.py", line 127, in run_backward_migrations
File "south_utils\run_migrations.py", line 45, in run_migration_command
File "site-packages\django\core\management\__init__.py", line 120, in call_command
File "site-packages\django\core\management\base.py", line 445, in execute
File "site-packages\django\core\management\commands\migrate.py", line 222, in handle
File "site-packages\django\db\migrations\executor.py", line 112, in migrate
File "site-packages\django\db\migrations\executor.py", line 168, in unapply_migration
File "site-packages\django\db\migrations\migration.py", line 162, in unapply
File "site-packages\django\db\migrations\operations\fields.py", line 206, in database_backwards
File "site-packages\django\db\migrations\operations\fields.py", line 201, in database_forwards
File "site-packages\django\db\backends\base\schema.py", line 484, in alter_field
File "site-packages\django\db\backends\postgresql_psycopg2\schema.py", line 113, in _alter_field
File "site-packages\django\db\backends\base\schema.py", line 656, in _alter_field
File "site-packages\django\db\backends\base\schema.py", line 111, in execute
File "site-packages\django\db\backends\utils.py", line 64, in execute
File "site-packages\django\db\utils.py", line 98, in __exit__
File "site-packages\django\db\backends\utils.py", line 64, in execute
OperationalError: cannot ALTER TABLE "organization_enterpriseuser" because it has pending trigger events

<br>

Version Introduced

4.5.10

<br>

Platform

ESM with Postgres 9.2

<br>

Steps to reproduce

  • Setup ESM with Postgres 9.2
  • Install 4.5.10 or later
  • Add a new user to ESM
  • Downgrade ESM to 4.5.9 or earlier

<br>

Expected result

Successful downgrade.

<br>

Actual result

Failed downgrade with the error above

<br>

Work Around

  • Connect to db
  • Set ‘last_login’ for all users in table ‘organization_enterpriseuser’

<br>

Version Fixed

4.5.17