Configuring exacqVision S-Series Enterprise System with LSI RAID Controller with all JBOD Disks

exacqVision S-Series systems with LSI RAID controller running exacqVision Server 6.4.x display an empty Network tab on the Storage page if all disks are configured for JBOD. To fix this issue, complete the following steps:

  1. On the S-Series system, download the udev_gen.sh script (attached below).
  2. cd to the location where the script was downloaded and run sudo ./udev_gen.sh.

The script will request storage updates from the kernel, and the disks should appear on the Network tab.