Axis plugin motion detection alarm event might not expire

Description

Setting a Record Video via Video Motion Event will not clear on an Axis Q6114-E camera running Edge software.

<br>

Tested Version

Edge 7.6.1.93449
Firmware 6.20.1
Client 7.6.4.94409

<br>

Platform

Edge

<br>

Steps to reproduce

  • Set a Motion Window on the camera via the Client
  • Confirm Motion Detection is functional
  • Create a new Event in Event Linking – Video Motion > “Motion Test” > Record Video > Pre set to 1 > Post set to 1 > Apply
  • Trigger motion on camera

<br>

Expected result

  • Motion triggers a red border based on the Event. The event should clear 1 second after motion has ceased being detected (based on Post-Trigger timing).

<br>

Actual result

  • The red border only clears when the 127.0.0.1 input is disconnected and re-connected to the Edge server.
  • Deleting the Event while the border is present does not clear the border.
  • Setting the schedule to Event Only has no effect.
  • Soft Triggers still function as expected

<br>

Fixed Version

7.9.16.99811