Additional Linux resources needed for larger installations

Description

  • Crashes found during restarts were traced back to insufficient file descriptors.
  • On larger installations we need to tune the linux server by allowing more file descriptors for our process.
  • The problem has been seen on systems with as few as 117 streams when storage rules are in effect.

<br>

Version Introduced

From beginning, scaleability issue.

<br>

Platform

Linux 32, Ubuntu 8.04,12.04,14.04

<br>

Steps to reproduce

Add cameras and streams and encoders with storage rules until restarting serve causes crash.

<br>

Expected result

No crash

<br>

Actual result

Server crashes during startup, restart or on scan, adding cameras or storage rule addition in various locations.

<br>

Work Around

Edit /etc/init.d/edvrserver start script – Add “ulimit -n 4096” in start section before line starting dameon.

<br>

Version Fixed

Unknown

<br>

Keywords

File Descriptors SEGFAULT SIGABRT SIGPIPE crash on startup