ESM needs to use port and address when building xdv for client

Description

If multiple servers share the same IP but have different ports. ESM will remove additional servers with same IP, only using one of the servers. It should include all of these servers.

<br>

Tested version

4.9.23

<br>

Platform

All

<br>

Steps to reproduce

Add multiple servers on ESM with same IP Address and different port numbers Sync ESM with thick client

<br>

Expected result

All servers on ESM should be synced to thick client

<br>

Actual result

For server with the same IP address and different port numbers, only one server on that IP is synced to the client

<br>

Work around

There is no known work around for this issue

<br>