Description
Even though the default max user name length on Django base classes is set to 30, ESM code attempts to override it with a max length of 255. However, while actually trying to create user names longer than 30, ESM fails with the database save length check error. For example, this error can be recreated when attempting to login with a LDAP, with ESM trying to create long user name ‘abcdefghijklmno@cfsad.com (domain)’ in the database
<br>
Tested version
4.9.23
<br>
Platform
All
<br>
Steps to reproduce
Attempt to login into ESM from the client’s ‘Synchronize with ESM’ page using a LDAP name that is longer than 25 (will be > 30 by the time ESM appends ‘(domain)’ to the user name).
<br>
Expected result
User login succeeds
<br>
Actual result
User login fails with a client pop up “Please check your URL”.
<br>
Workaround
None
<br>