“Can change password” should be locked as false for LDAP users

Description

LDAP users (or LDAP administrators) have all the tools needed to administer their LDAP account credentials. We do not provide (or need to or want to provide) any tools to administer LDAP credentials.

This evServer fix is a guard to block this setting in the xml. If config is sent to the server containing this value, it is removed. No evAPI changes are needed or expected.

<br>

Version introduced

v8.6.0

<br>

Platform

All

<br>

Steps to reproduce

  • Configure an LDAP user with Full Admin privileges
  • Connect as the LDAP user

<br>

Expected result

  • Change Password panel should be hidden
  • Actual result
  • Change Password panel is visible

<br>