Description
Server crashes when add Axis camera with date/time on the camera is set to sync manually or with computer time.
<br>
Version introduced
8.6.1.115070
<br>
Platforms
All
<br>
Steps to reproduce
- In the camera web page, change the “Time mode” to either manual or with computer time in “Date & Time Settings” page.
- connect Axis camera to 8.6.x server.
<br>
Expected result
NTP is sync either to server or override setting.
<br>
Actual result
Server crashes.
<br>
Workaround
Manually set “Time mode” to “Synchronize with NTP server” option.
<br>
Version fixed
8.7.8.115465
<br>