Why don’t I see the layout icons on top of my screen?

This can happen if you have highlighted the Views icon on the left hand side of the live view.  Since a View has a predefined layout, there is no option to choose a new one from the top menu.  If you would like to change the layout and choose cameras for it, you will need to click on the “Cameras” icon on the left hand tree near the bottom.

This can also occur if a user has accidentally pressed the F8 key at the top of the keyboard, which toggles the toolbar from being displayed or hidden.

In some cases you may have an older version of client in which there was a feature that is no longer enabled that limited the views to the number of connected cameras.  A simple client upgrade will solve this.

<br>