Where are ExacqVision Groups and Views Stored?

Views and Groups are stored on the the relevant ExacqVision servers. For example, if you create a view named “East Side Entrances” that has Camera A from Server 1 and Camera B from Server 2, the group ID and name are stored on both Server 1 and Server 2. Also, Camera A’s membership in “East Side Entrances” is stored on Server 1 and Camera B’s membership in “East Side Entrances” is stored on Server 2.

Thus, if the integrator connects his Client at home to Server 1, he sees a group named “East Side Entrances” containing Camera A without any need for configuration or file transfer. If he then connects to Server 2, Camera B is also seen in “East Side Entrances”.

<br>