What is the limit on the number of Event Linking entries I can create?

There is no programmed limit to the number of Event Linking entries you can create.

However, if you set up more than 50 Event Linking entries, it is a good idea to deselect the Log checkboxes displayed to the left of the event listing. The log file can grow to an unstable size if you do not do this.

If you want to create more than 500 entries, please contact Exacq Technical Support for guidance. 

<br>