If you select the SQLite database when installing or upgrading exacqVision Enterprise Health Manager (eVEHM) in Windows Vista or Windows 7 and install the database in or under the Program Files directory, you will have to right-click and select Run as Admin every time you use the eVEHM Client. The Client requires elevated privileges to read and write to a database in or under Program Files.
To avoid selecting Run as Admin every time you run eVEHM Client, save the database file to a directory that is not under Program Files.

<br>
Upgrading-exacqVision-Enterprise-Health-Manager-SQLite-Database-Access.pdf