Starting iSCSI on Startup with Linux Systems

After you reach the point where everything is logged in (you are able to type iscsiadm –m session and get output), following is the generic syntax:

iscsiadm -m node -T <targetname> -p <ip:port> –op update -n node.conn[0].startup -v automatic

<br>

The parameters between < and > are substitutions.

The syntax for persistent binding devices discovered on an internal connection under Ubuntu would look like this:

iscsiadm -m node -p 172.16.16.1 –op update -n node.conn[0].startup -v automatic

<br>

Here’s a more complete breakout, with examples from another system with two volumes (vol1-test and vol2-test), each with two connection paths, to log in to:

root@xxx:/etc/iscsi# iscsiadm -m node -l

Login session [iface: default, target: iqn.2003-01.com.pivot3:raige.vol:34xen.defaultpool.vol1-test.600176c30c272e438f96ea2d48669f4a, portal: 10.4.15.164,3260]

Login session [iface: default, target: iqn.2003-01.com.pivot3:raige.vol:34xen.defaultpool.vol1-test.600176c30c272e438f96ea2d48669f4a, portal: 10.3.15.102,3260]

Login session [iface: default, target: iqn.2003-01.com.pivot3:raige.vol:34xen.defaultpool.vol2-test.600176c34e91735e80bcbba748669f4a, portal: 10.4.15.164,3260]

Login session [iface: default, target: iqn.2003-01.com.pivot3:raige.vol:34xen.defaultpool.vol2-test.600176c34e91735e80bcbba748669f4a, portal: 10.3.15.102,3260]

<br>

The following is used for persistent binding to just the first volume, by target name:

# iscsiadm -m node -T iqn.2003-01.com.pivot3:raige.vol:34xen.defaultpool.vol1-test.600176c30c272e438f96ea2d48669f4a –op update -n node.conn[0].startup -v automatic

root@xxx:/etc/iscsi# /etc/init.d/open-iscsi restart

 * Disconnecting iSCSI targets                                                  Logout session [sid: 1, target: iqn.2003-01.com.pivot3:raige.vol:34xen.defaultpool.vol1-test.600176c30c272e438f96ea2d48669f4a, portal: 10.4.15.164,3260]

Logout session [sid: 2, target: iqn.2003-01.com.pivot3:raige.vol:34xen.defaultpool.vol1-test.600176c30c272e438f96ea2d48669f4a, portal: 10.3.15.102,3260]

Logout session [sid: 3, target: iqn.2003-01.com.pivot3:raige.vol:34xen.defaultpool.vol2-test.600176c34e91735e80bcbba748669f4a, portal: 10.4.15.164,3260]

Logout session [sid: 4, target: iqn.2003-01.com.pivot3:raige.vol:34xen.defaultpool.vol2-test.600176c34e91735e80bcbba748669f4a, portal: 10.3.15.102,3260]

                                                                         [ OK ]

 * Stopping iSCSI initiator service                                      [ OK ]

 * Starting iSCSI initiator service iscsid                               [ OK ]

 * Setting up iSCSI targets

Login session [iface: default, target: iqn.2003-01.com.pivot3:raige.vol:34xen.defaultpool.vol1-test.600176c30c272e438f96ea2d48669f4a, portal: 10.4.15.164,3260]

Login session [iface: default, target: iqn.2003-01.com.pivot3:raige.vol:34xen.defaultpool.vol1-test.600176c30c272e438f96ea2d48669f4a, portal: 10.3.15.102,3260]

                                                                         [ OK ]

<br>

NOTE: This just pulls in that target (vol1-test). Further, we could add by –p 10.3.15.164 in a second operation and pull in one other connection that the above did not add, for vol2-test on an IP basis (or, if this were the first operation, it would have added one connection to each volume). To turn off automatic binding for a given connection, you would use –v manual instead of -v automatic.

<br>

Also, none of this takes effect until the iSCSI daemon is restarted.

<br>

Starting-iSCSI-on-Startup-with-Linux-Systems.pdf