Description
Exacq built systems with redundant power supplies will emit an audible alarm in the event of a power failure. Here is how to silence the various models so you can enjoy peace and quiet while determining the cause of the failure.
Product
- Exacq-built Servers
Solution
The following photos show the location of the mute button on different models:
2U IPS Z Series – Newer Models

2U IPS Z Series – Older Models

3U IPS Z Series

4U IPS and Hybrid Z Series

<br>