Joystick Z-Axis on Mac-based exacqVision Client

When using a joystick on Mac-based exacqVision Client software, Z-Axis operations do not work correctly. On an exacqVision Surveillance Keyboard (and most other devices), the joystick’s Z-Axis is mapped to the action of twisting the joystick, which is used to control zoom functions.

On some keyboards, zoom functionality can be mapped to a programmable button. See the keyboard manufacturer’s documentation for information about programming buttons.

<br>

Joystick-Z-Axis-on-Mac-based-exacqVision-Client.pdf