Supporting HDD SMART Data on Third-party Hardware

When installing ExacqVision Server software, including its System Management plugin on third-party hardware, you should aim to use a RAID controller used in Exacq manufactured systems, which include:

  • Broadcom MegaRAID 9670
  • Broadcom MegaRAID 9560
  • LSI MegaRAID 9670
  • LSI MegaRAID 9560
  • 3ware 9750
  • 3ware 9650

If a different controller (or no drive controller) is used, the behavior of the system will vary.

SMART data from a drive controller is handled by Smartmontools. For more information, visit theĀ Smartmontools wiki.

<br>