To enable mutlistreaming on compatible Pelco cameras, you must adjust settings in the camera’s web interface. Select the A/V Streams tab and ensure that both streams are configured for the H264 Compression Standard.
NOTE: If the secondary stream is greyed out and not available for changes, adjust the primary stream settings until the secondary stream settings are no longer greyed out.

<br>
Enabling-Multistreaming-on-Pelco-Cameras.pdf