Can I run a Silent Install of ExacqVision?

ExacqVision Server and Client EXE installers adhere to the normal NSIS installation options.

/S runs the installer silently.for silent.
Example: exacqVision_23.0.3.6_x64.exe /S

/D changes the installation directory. While the default directory is recommended, you may use this option to override it to install in another directory.
Example: exacqVision_23.0.3.6_x64.exe /S /D=C:\Program Files\MyCustomDirectory

More information about NSIS options can be found within NSIS documentation at:
http://nsis.sourceforge.net/Docs/Chapter3.html.

<br>

Additionally, the ExacqVision Desktop Client is provided in an MSI installer for Windows deployments, which provides silent installation using the /quiet parameter.

Example: msiexec /i exacqVision_23.03.3.6_x64.msi /quiet

<br>