Adding/Configuring Locales on Ubuntu Linux

For Ubuntu, adding a new locale (language) is a two-step process. First, determine the UTF8-encoded locale name, then generate the UTF8-encoded locale.

<br>

Determine Locale Name

Open a command line window and type:

less /user/share/i18n/SUPPORTED

This will list all of the locales Ubuntu supports. Scroll down to find the one that matches the ISO 639-1/ISO 3369-1 language codes of the language you are wanting to add.

Please be aware that some of the locales will not have a suffix (look closely – there is no period (‘.’) between the xx_YY language code and the following characters). Others will have a suffix of ‘.UTF-8.’ Still others will have suffixes like ‘@euro’ and ‘.EUC-KR.’ For ExacqVision, you must use the locale with the ‘UTF-8’ suffix.

For example, Irish in Ireland has these three locales:

...
ga_IE.UTF-8 UTF-8
ga_IE ISO-8859-1
ga_IE@euro ISO-8859-15
...

The first one has a ‘UTF-8’ suffix and should be used. The second and third ones do not have the ‘UTF-8’ suffix and should NOT be used.

<br>

Generate Locale

Since we’ve now determined the proper locale to generate, head back to the command prompt and type (once for each locale you wish to generate):

sudo locale-gen ga_IE.UTF-8

To actually trigger Ubuntu to generate the locale(s), type:

sudo dpkg-reconfigure locales

To verify that the locale(s) were generated, type:

locale -a

<br>

Change the Locale

For any given run of any program

Also, you may run the exacqVision Client from the command line preceded by an env setting. For example:

env LANG=es_CL.utf8 /usr/local/exacq/client/edvrclient

will cause the exacqVision Client to run with the Chilean Spanish translation.

<br>

Permanently

To change the locale, you may change the entire operating system by going to System->Administration->Language Support and changing the default language dropdown. This will require a reboot.

<br>