Why doesn’t my ExacqVision system capture the exact frame rate configured for my camera?

The Frame Rate setting on the ExacqVision Camera Recording page, or the individual Camera Settings page, is a requested setting; this frame rate is not guaranteed.

Although the ExacqVision software is designed to capture every frame that it receives from the camera, the actual recorded frame rate can be reduced by network issues, firmware, scene dependencies, resolutions, and other settings.

The range of settings available for the Frame Rate selection is based on the frame rates that the camera can be expected to provide.

<br>