If live video from a Bosch ONVIF camera displays pixelization in exacqVision Client, complete the following steps:
- Browse to the camera’s advanced mode Encoder Profile page.
- Ensure that IP is selected in the GOP Structure drop-down list.
- Ensure that the I-frame Distance slider is configured for a low number (10, for example).
- Ensure that I-frame Quality and P-frame Quality are set to Auto.

<br>
Pixelated-Video-on-Bosch-ONVIF-Cameras.pdf