NOTE: Enterprise licensing is required to create child maps.
To create a child map, open the ExacqVision Desktop Client and complete the following steps:
- Click the Maps node on the navigation tree to open the Maps page.<br><br>
- From the maps tree, click to highlight an existing map you wish to be the parent map to the child map you are about to create.<br><br>
- Click the New button below the maps list panel.<br><br>
- Name the child map.<br><br>
- Give the map a description (optional).<br><br>
- Click Map Image and load the image you want to use.<br><br>
- You also have the option of using the Add Icon button to upload a thumbnail image to display in the map tree for this map. The icon drop-down allows you to select from previously used icons.<br><br>
- From the Available Items panel drag the appropriate cameras to their position in the map.<br>
NOTE: You may also drag input triggers, soft triggers, output alarms, audio devices, serial data streams, web panels, and access control integrations onto maps.<br><br> - Click Apply.<br>
NOTE: If you do not add at least one device to the map, you cannot click Apply.<br><br> - The parent map now lists this map as a child map.<br><br>
- Repeat steps 2-9 to create additional child maps. <br><br>
- Returning to the parent map, you may drag the child map from your list of Available Items onto it allowing users to navigate from the parent to the child map.
See also: Maps from our Video Library<br><br>

<br>