Themes
The ExacqVision Desktop Client added support for Themes in version 8.4. Since version 20.03, the Client will default to the Light theme upon installation.
The Theme may be selected by navigating to the Client node from the left-hand navigation panel.


Changing the selected theme will prompt you to restart the Client to display the new theme.



<br>
Alternative Methods
Prior to Client version 8.4 the Client configuration page in ExacqVision allowed you to change certain aspects of the ExacqVision Client software, such as the color of recording indication borders. However, the background color in ExacqVision Client was based on operating system settings.
To change the overall appearance of ExacqVision, complete the following steps in Windows (steps and options might vary slightly between Windows 7 and Windows 8):
- Open Control Panel.
- Select the Personalization option, and then Change the Theme.
- Select Windows 7 as the theme group, and then Windows 7 Basic as the theme.
- Select Windows Color.

In the Window Color and Appearance dialog, select colors as desired.

In the following example, the background has been changed to dark grey using Windows. The motion recording border has been changed to dark blue and the borders between video windows have been hidden using ExacqVision Client.

<br>