The streaming profile of ONVIF (Profile S) provides a standard interface for streaming video and audio between conformant devices (cameras or encoders) and clients (VMS). The ExacqVision VMS is listed as an ONVIF Profile S-conformant client.
Extensive testing with a wide variety of ONVIF Profile S-conformant cameras has revealed enough inconsistency that Exacq does not explicitly declare support for all Profile S cameras for use with ExacqVision. Only the IP cameras listed in the Exacq IP Camera Integration database are officially compatible and supported for use with ExacqVision. Cameras not listed in the camera database should not be considered compatible with ExacqVision, even if they are Profile S-conformant.
If you are interested in using an ONVIF Profile S-conformant camera that is not listed in our camera database, please submit an integration request on the IP camera integration web page by clicking “Can’t Find Camera?”

<br>