USB I/O Linux installer will not run when double-clicked

Affected Platforms

Linux 12.04 and 14.04
<br>

Symptom

You receive the following error when installing the USBDio installer in Linux:

Could not open ‘exacqVisionDio.deb’ The package might be corrupted or you are not allowed to open the file. Check the permissions of the file.
<br>

Resolution

You will need to install the package via the command-line. Here are the steps to install the package:

  1. Place the package ‘exacqVisionDio.deb’ on the desktop
  2. Open the terminal. Applications –> Accessories –> Terminal
  3. Run the following command:
    sudo dpkg -i ~/Desktop/exacqVisionDio.deb
  4. Enter your password when prompted

<br>