If you see motion images from a Bosch camera that appear to be out of order, the issue can often be resolved by selecting a different setting for the camera’s GOP Structure. To change the setting, complete the following steps:
<br>
- Open the camera’s web configuration page by entering it’s IP address in an Internet browser.
- Open the Settings page and select Advanced Mode in the menu on the left.
- Select the Cameras entry and then Encoder Profile.
- Click the Expert Settings button to reveal additional options, including GOP Structure.
- Make sure IP (which stands for I Frames, B Frames, and P Frames) is selected in the GOP Structure drop-down list.
- Click Set to enable the selected settings.
<br>

<br>
Motion-Frames-Out-of-Order-on-Bosch-Cameras.pdf