Georgia Standard Time Zone Incorrect

In a Windows environment, the Georgia Standard Time zone displays correctly in the Windows “Time Zone Settings” drop down box as:
(UTC+04:00) Tbilisi

However, the exacqVision Software may display it incorrectly as:
(UTC+03:00) Tbilisi

This is because the Windows Registry may still reference this time zone as +03:00. The attached registry patch will correctly set the Tbilisi time zone to +04:00 in the Windows Registry. It is recommended to backup your Registry before applying this patch. Fore instructions click here.

NOTE: This patch will not help if you are running the 32-bit exacqVision Server service on a 64-bit Operating System.

<br>

Georgia-Standard-Time-Zone-Incorrect.pdf