- Insert USB drive in the front or rear USB ports of the Exacq Server.<br><br>
- From the Search page, follow the directions for finding and marking the start and end points of the video desired.<br><br>
- Chose the Download and Export button from the toolbar. Shown, below, are the icons in Light, Dark, and Classic themes.
<br><br>
- When running the exacqVision Client without administrative privileges, users may only export to the exacqVision Files directory within their user account or a USB drive. The below example shows the appearance of this window where the USB drive is volume D:\. Clicking into D:\ will open the USB volume for exporting.
<br><br>
- When running the exacqVision Client with administrative privileges, users have the ability to select from any directory on the system, including the USB drive. Click into the USB drive to select it as the location for exporting.
<br>
NOTE: If using Linux, navigate to the USB_KEY folder. This is your mounted USB device.<br><br> - You may accept the default video File Name or create your own.<br><br>
- Choose Save and your selected video will be exported to the USB device.
<br>